ECAT.TXDONETIME

Description

This parameter allows viewing and recording of the Distributed Clock (DC) time when the drive completes updating the input packet data (TxPDO). This ideally occurs prior to the ECAT.RXDONETIME for proper control. If it occurs after, ECAT.INPUTSHIFTU can be adjusted to specify a time after the Phase-Locked Loop (PLL) reference for the drive to prepare inputs.

Context

See Synchronization.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read Only

Units

ns

Range

0 to 4,294,967,295 ns

Default Value

N/A

Data Type

Integer
See Also ECAT.POSLOOPTIME, ECAT.RXDONETIME, ECAT.RXIRQTIME, ECAT.SYNC0TIME

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT variants: AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ECAT.TXDONETIME

4300h

03h

Unsigned32

-

-

Read only

Yes